hello
iam working on a new design which i will be using the uc3637 as a class d amp, o i will set the device to produce two 50% duty cccle lets say at
25 khz, okay from here the two outputs will go to a half bridge driver which will be the ir 2110 are another later part for the driving og the power devices,
now what i need once the sinewave has came across the power magnetics i need a way to sync multiple uc3637 devices for freq and output sinewave ampltd. which will be 115 vac from 60hz to 400 hz
i need to make are have one unit /are module as the master and have lets say the other three modules sync to that so i will have combined output power
could you give me some ideas on how to sync multiple devices together for this design, i will be sampleling the output directly from the out put via a small feedback transformer into a ad633 multiplier for loop control, let me no as soon as possible