This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H5001-SP: Commercial Grade Available

Part Number: TPS7H5001-SP
Other Parts Discussed in Thread: UCC28251, , TPS7H5008-SEP, TPS7H5005-SEP

Tool/software:

Hello,

is there are commercial grade variant of the TPS7H500x or a derived part? The 2MHz operation, current sense input redundant/interleaved operation sets it apart from other parts available.

  • Hello,

    The TPS7H500X-SP family is a grounds up design of a space grade controller.
    This means there is no commercial equivalent as it was designed for specifically space grade applications.

    Thanks,
    Daniel

  • Hello,

    could you recommend an alternative part? All I see that is halfway comparable is the UCC28251 which realistically operates <1MHz and, at least from the datasheet, lacks some capabilities with regard to current mode control as well as the simulation models where the TPS7H500x provides a full transient model.

    Best Regards,

    M.

  • Hey M.

    The UCC28251 was used as the commercial basis for the part.
    How much the TPS7H5001-SP is different than the UCC28251 shows how much was engineered from the grounds up.

    There are lower space grade versions of the part in the TPS7H5005-SEP through TPS7H5008-SEP.
    There are EM versions of the part meant for prototyping.
    I do not know of a commercial part that is close to the TPS7H5001-SP.

    Thanks,
    Daniel

  • Hi,

    thanks for conclusively answering that. I see that the two parts are quite similar (except for speed unfortunately) so I'll live with the switching speed limit and work around the small issues with current feedback. Using a space qualified part is cost-prohibitive.

    Thanks again,

    M.

  • Welcome

    Thanks,
    Daniel