This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM365R6: Vias at VIN(3pin) and SW(6pin) in the LAND PATTERN EXAMPLE

Part Number: TPSM365R6

Tool/software:

Dear Specialists,

My customer is considering TPSM365R6V5 and has a question.

I would be grateful if you could advise.

---

I have a question about the pattern for the TPSM365R6V5RDNR.

Regarding the VIN3 pin and SW6 pin,

There are no vias in the layout example in 10.4.2 Layout Example.

On the other hand,  there are two vias for each in the land pattern example.
・What are these vias for?
・Are these vias necessary? I think the vias are large compared to the pattern.

---

I appreciate your great help in advance.

Best regards,

Shinichi