Tool/software:
Hello,
We have designed a power evaluation board to evaluate the PMIC TPS65313-Q1 for an Automotive ECU application.
Our design closely follows the reference circuit provided in TI’s evaluation board for this PMIC.
When powering the board, all voltage outputs—3.3V, 1.2V, and 5V—are within the expected range.
However, during a load test, we observed an issue with the 3.3V output: it drops and loses regulation when the load current exceeds approximately 890 mA.
The load test was performed using a rheostat, and the voltage drop occurred when the resistance was set to 3.9 ohms or lower.
Could you please review the attached circuit and provide guidance on how to resolve this issue?
Input voltage :- 12V DC
Thank you for your support,
Jacob