Part Number: UCC21750-Q1
Tool/software:
Hello
The AIN Input has a 200 uA of current from Vdd which is +18V in my application.
While using an NTC of say 10K @ 25*C with Beta of 3984, at low temperatures
the Resistance is over 30K resulting in a voltage of 6 V & above at AIN.
The Specs mention a Max voltage as 5V.
Above 4.5 V the PWM may go above 88%, which is of concern to me.
But otherwise do I need to bother about exceeding 5V at AIN
such as zener clamping?
Thanks and regards
Varun