Other Parts Discussed in Thread: TPSM82816
Tool/software:
Thank you for your continued support.
I have an additional question.Cause_of_LMZ10504_failure_20241223.pdf
The LMZ10504TZX-ADJ/NOPB no longer outputs an output voltage. I removed the part and measured the resistance of the output (VOUT pin) and GND pin, and found that they were shorted (1.08Ω).
The operating conditions are: input voltage: DC+5V, output voltage: DC+3.3V, output current: 1A, operating environment: 25°C. I have also attached a circuit diagram using this part for reference.
So, I have a question.
(1) Are there any factors that could cause the output (VOUT) to be shorted?
(2) Can the input and output capacitors be damaged due to insufficient capacity?
(3) If the part is damaged due to (2) above, can the output (VOUT) be shorted?
Thank you for your advice.