Tool/software:
Dear Specialists,
I am proposing the "LMR51435SDRRR" to a customer as a replacement for the MAX42403AFLB+.
The customer has a question about thermal resistance.
I would be grateful if you could advise.
---
The θj-a is 47.4°C, which is better than the ADI product. That's a good point.
The LMR51435 has θj-c(top)=44.6°C, while the MAX42403AFLB (ADI) has θj-c=21°C, so there is a difference.
I am concerned about the difference.
What is causing this difference? (Is there a difference in measurement conditions?)
Why are the θj-c values different even though the θj-a values are almost the same?
---
I appreciate your great help in advance.
Best regards,
Shinichi