Part Number: UCC14241-Q1
Other Parts Discussed in Thread: UCC21710
Tool/software:
Hi,
I am trying to use the UCC14241 integrated power supply along with the UCC21710 isolated gate driver for driving SiC MOSFETs. The desired voltage rails are +16V (Vdd - COM) and -4V (Vee - COM).
The reason for this post: I'm getting conflicting component results when manually calculating Cout1B, Cout2, and Cout3 as compared to the gate drive requirements based on the total gate charge and required total bypass capacitance.
As a result, I'm trying to resolve the final component selection so I can progress with my system design.
General parameters I have provided as inputs for calculations using Equations 1, 2, 4, 7, and 8 from datasheet of UCC14241:
- Desired Vdd_COM voltage = +16 V
- Desired Vee_COM voltage = -4 V
- Qg = 0.45 uF
- I_max_power = 10 A (Using peak drive current capability supported by UCC21710, from datasheet)
- I_vdd_com = 5 mA (from UCC21710 datasheet)
- I_com_ee = 5 mA (from UCC21710 datasheet)
- deltaV_Vdd_COM = 0.5%
- Desired C_VDD_COM_EQ = 10 uF
Using above values and the UCC14241 datasheet equations, I calculated the following capacitance values:
- Cout1B = 5.37 uF
- Cout2 = 1.52 uF
- Cout3 = 6.08 uF
To check the equivalent C_VDD_COM_EQ capacitance, I use equation (1) from the UCC14241 datasheet. The result is 4.37 uF. However, this is much less than my desired value of 10 uF as shown above.
I have the following questions outlined below, so I can progress with my design.
Questions:
- Can I please get some help in verifying if the parameters I have used above are correct given the dual output voltage rails requirement? I do not have access to the SIMPLIS full version so I can't simulate it myself to validate the design before PCB implementation.
- My calculated total bypass capacitance (Vdd_com) = 10 uF to meet the voltage droop and gate charge requirement. However, the above values do not provided the needed capacitance. Can I get help in understanding how to meet the desired bypass capacitance value?
- For equations 19 and 20, how do I define the value of V_FBVDD and V_FBVEE?
My entire system design has been halted due to this issue. As a result, I would really appreciate some help in resolving this problem at your earliest convenience.
Thank you,
Kartavya Agarwal.