Part Number: LM25149-Q1
Other Parts Discussed in Thread: LM5177
Tool/software:
Hi,
My system requires an input voltage range of 7-18V and an output voltage range of 15-28V. I need to be able to set the output current to a fixed 3A. I should be able to adjust the input current limit. UV/OV protections should be addable. I need to be able to enable/disable the system via a microcontroller. The system should also allow the use of external MOSFETs. Can you recommend a suitable DC-DC controller IC?
Best Regards.