Tool/software:
Hi team,
Could you help provide TLV76050 V.S LM7605N3 comparesion table?I want to know where our advantage. Thanks
https://datasheet4u.com/datasheet-pdf/CYStech/LM7605N3/pdf.php?id=1341182
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Could you help provide TLV76050 V.S LM7605N3 comparesion table?I want to know where our advantage. Thanks
https://datasheet4u.com/datasheet-pdf/CYStech/LM7605N3/pdf.php?id=1341182
Jimmy,
Please see comparison below:
|
TLV760 |
Select an GPN |
Iout(Max)(A) |
0.1 |
0.2 |
Vin(Max)(V) |
30 |
30 |
Vin(Min)(V) |
4.2 |
4.85 |
Vout(Max)(V) |
15 |
5.15 |
Vout(Min)(V) |
3.3 |
4.75 |
Fixed output options(V) |
3.3, 5, 12, 15 |
5 |
PSRR @ 100 |
45 |
40 |
Noise(uVrms) |
100 |
42 |
Accuracy(%) |
4 |
- |
Dropout voltage |
700 |
1700 |
Iq(Typ) |
2 |
- |
Output capacitor type |
Ceramic |
Ceramic |
Thermal resistance |
270 |
417 |
Operating temperature |
-40 to 125 |
-40 to 150 |
Package size: mm2 |
7 mm2: 2.37 x 2.92 (SOT-23|3) |
7 mm2: 2.37 x 2.92 (SOT-23|3) |
Rating |
Catalog |
Catalog |
Thanks,
Prakash L