This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH-POWER-DESIGNER: require a battery charger

Part Number: WEBENCH-POWER-DESIGNER

Tool/software:

We require a battery charger with the following specifications:

Output Supply:
- Voltage: 13.5V
- Current: 3A
- Mode: Constant Current (CC) / Constant Voltage (CV)

Input Supply:
- Voltage: 110-240VAC
- Frequency: 50Hz/60Hz

Please provide a suitable battery charger that meets these requirements.

shankar kanki

  • Hi Shankar,

    There is no single battery charge IC that takes AC input.  All of the battery IC's need a DC input.  A multi-chip reference design with an AC/DC converter followed by a battery charger is required.  The have some questions:

    1. What is battery type, LiIon, lead acid, etc.?

    2. What is the end application or at least the high level category form the list below for your application?  I need this info in order to forward your request to the correct reference design team.

    Regards,
    Jeff