Part Number: TPS61240
Tool/software:
Hi! First time here,
i'm designign a boost converter for a small PCB that i'm doing: it has an ATtiny MCU and 25 addressable LEDs and the whole board is powered by a coin 3V battery (CR2032).
I've did some tests with the latest prototype and the whole board with the current firmware draws about 15-25mA, which is a bit too high for this type of battery but it should be okay.
I would like to have a stable 4-5V output with an input range that varies between 2.3 and 3.3V (CR2032).
Here's my current schematic for the step-up converter:
Does this approach make sense for the components and requirements? Are there any optimizations or potential issues I should look out for (e.g., inductor selection, capacitor sizing, etc.)?
Jack