Other Parts Discussed in Thread: UCC28070A, , UCC28019A
Tool/software:
Hello-
I'd like to implement a Buck PFC to convert 3-phase AC power (either 208 or 480 in separate designs) to ~200 Vdc at maximum of just over 2kW. According to sluaao8 the upper power limit of UCC29910A would be at about 2kW but suggests the UCC28070A in interleaved PFCs for higher than 2kW, but the application information on the UCC28070A datasheet shows a boost configuration. Can a UCC29910A based buck PFC be pushed to this kind of output voltage and power rating? If not, are there higher power interleaved buck PFC options?
Thanks