零件编号:BQ27Z746
工具/软件:
我有一个问题困扰我很久了,我知道在数据内存=>Protections=>HW threshold targets可以设置OCD的阀值,比如设置成-28mV,我选用的Rsns电阻是20mohm,当电阻两端电压接近-20mV(约0.9A)时,就会触发OCD保护,关断输出。这与规格书的可设置范围(-4~-100mV)不符。(为了防止软件OCD提前保护了,我将电流特意设置成-2400mA),我做了验证,Rsns无论多大电阻,它两端电压的都是接近20mV时,就会触发保护,能告诉我这是怎么回事吗,需要如何处理才能使Rsns上电压大于-20mV不会被关断,谢谢