Tool/software:
Hi,
May I ask why does the 1V output disconnect for 4ms every approximately 74 seconds when a 2.2k pull-down resistor is already connected to the WD pin.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
May I ask why does the 1V output disconnect for 4ms every approximately 74 seconds when a 2.2k pull-down resistor is already connected to the WD pin.

Hello Li,
More information is needed from your side before I can provide a detailed answer:
BR,
Nicholas McNamara
Thanks for your reply! I will explain these as following.
1. The full part number is LP877451A1RXVRQ1, the same as used in AWR29494.
2. The output voltage of three BUCKs are 1.8V, 1V and 1.2V respectively. All BUCKs has reset.
3. As figure attached before, there is a 4ms pull-down occurs every 74s and continues in a cycle until power is diconnected.
4. At the same time, I am also trying to suppress the restart by feeding the watchdog. Could you tell me what the register address corresponding to the watchdog is?
1. The full part number is LP877451A1RXVRQ1, the same as used in AWR29494.
2. The output voltage of three BUCKs are 1.8V, 1V and 1.2V respectively. All BUCKs has reset.
3. As figure attached before, there is a 4ms pull-down occurs every 74s and continues in a cycle until power is diconnected.
4. At the same time, I am also trying to suppress the restart by feeding the watchdog. Could you tell me what the register address corresponding to the watchdog is?
1. Thank you this helps confirm the watchdog long window, which is the 5 seconds which I see the time mark for
2. Which according to the shutdown sequence, they all should thank you for confirming
3. Okay, it's systematic, but do you know for a fact that this is being caused by the WD timing out? I see no evidence for this at the moment, so can you please readback the registers from 0x47 to 0x51, these are interrupt registers. Does the microcontroller stop sending the answers for the watchdog, can you show me the traffic that does this?
4. Please access the resource page that will link to the datasheet for more information, I can't say anymore: (resource link page here)
BR,
Nicholas