This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5811: LED Forward Voltage

Part Number: LP5811
Other Parts Discussed in Thread: LP5810, LP5813

Tool/software:

Hello Team,

Greetings !!!

This is regarding LP5811ADRRR. I have input voltage as 3.3V +/- 5%. The LED I wanted to drive is with maximum Forward voltage of 2.5V and maximum current of 30mA.

Given that the driver is boost in nature, will it work to drive the LED with 2.5V forward voltage ?

 Please refer the attachment.

Thanks and Regards

G R K Nagaraju