Other Parts Discussed in Thread: BQ25756, , BQ25758, BQ25751
Tool/software:
Hi all.
Trying to create my own design bq25758a-based to fast charge a bank of capacitors, even not "super-", just a set of ordinary with total capacitace ~10000uF. I need to support high-power pulses with freq ~50 Hz. Surely, during pulse bq25758 IC must be disabled (CE - high). So, the question is: what is duration between "charge enable" (CE - low) and "charge started" (full current output) for bq25758a? Cause for it's "sistership" bq25756 this time is too long for my application (~200ms - as I recognized from the datasheet).
Thanks a lot.