The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61378-Q1: Still see output voltage with EN low

Part Number: TPS61378-Q1

Tool/software:

Hello,

I used TI's Web-Bench to design a circuit that uses the TPS61378-Q1 and that takes 4.2 VDC from a single cell Li-ion battery and boosts it to 12 VDC with the enable pin high in accordance with the schematic shown below. This works. When the enable pin is low (0.0 VDC) the output voltage is 4.8 VDC. Please review my schematic and make suggestions.

Thank you,

Patrick