This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619E: BATFET turn off when VBAT present

Part Number: BQ25619E


Tool/software:

Hello,

Here is my test description:

  • Applied 3.8 VBAT and 5.0 VBUS
  • Bit 4 of REG0x07 BATFET_RST_WVBUS  = 0
  • Disable BATFET via bit 5 of REG0X07
  • Wait 10 seconds if bit 3 of REG0x07 is checked
  • BATFET turns off, charging stops but SYS is still 3.9 V

I was thinking, reading the datasheet, that this configuration would not turn off BATFET and stop charging when VBUS is present.

Can you confirm it is the normal behavior?

What is the difference between BATFET_RST_WVBUS=0 or 1?

Regards,