This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8865U-Q1: Recommended loop stability compensation components value

Part Number: LP8865U-Q1


Tool/software:

Hello,

My customer designing their LED driver circuits using LP8865U-Q1, and their design requirements are as follows.

Input voltage range:12V
LED string:36 LEDs(6series x 6para)
Output voltage:16.8-19.2V
Switching frequency:800kHz
Maximum LED current: 240mA
Inductor current ripple: 40%
Dimming type:PWM Dimming(Duty100%, fixed)

In their design, what CCOMP, RCOMP and RDAMP are recommended to have good loop stability?

Best regards,

K.Hirano