Tool/software:
We are using the BQ24296MRGER part in our design, but we have a safety circuit that disconnects the thermistor when the battery voltage drops too low.
Is there a way to override the CE (Charge Enable) and thermistor fault and enable charging only by configuring REG01[5:4]? Assuming CE and TS are not externally controlled, we need to bypass this restriction and enable the charger via the host.
According to specs:
A new charge cycle starts when the following conditions are valid:
• Converter starts
• Battery charging is enabled by I 2C register bit (REG01[5:4]) = 01 and CE is low
• No thermistor fault on TS
• No safety timer fault
• BATFET is not forced to turn off (REG07[5])