This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What is the minimum difference between input voltage and LED (string) voltage for TPS922055 / TPS922054 / TPS922053 / TPS922052 to regulate the output current?

Other Parts Discussed in Thread: TPS922052, TPS922055, TPS922054, TPS922053

What is the minimum difference between input voltage and LED (string) voltage for TPS922055 / TPS922054 / TPS922053 / TPS922052 to regulate the output current?

  • For TPS922055 / TPS922054 / TPS922053 / TPS922052 to regulate the output current to the target value, you should make sure that LED (string) voltage < input voltage.

    For TPS922055 / TPS922054 / TPS922053 / TPS922052 to regulate the output current to the target value most accurately and consistently, you should make sure the voltage of the CSP pin > 2V. That is to say, you should make sure that input voltage - LED (string) voltage > 2V.