Part Number: TPS62932
Tool/software:
V(IN_MAX)=12V, f_sw=500KHz,I(OUT_MAX)=2A,V_OUT=6V,K=0.4=(∆I_L)/I_(OUT_MAX)
I calculated the inductor base on above condition.
Why in webench showing 12 uH? But I calculate using formula it coming 8.2 uH?
Additional question, If the load current is 0.5A, Should I use 2A rated current or 0.5A load current in formula to calculate?Should I use 2A rated current or 0.5A load current in webench input?