This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62932: inductor Calculation

Part Number: TPS62932

Tool/software:

V(IN_MAX)=12V, f_sw=500KHz,I(OUT_MAX)=2A,V_OUT=6V,K=0.4=(∆I_L)/I_(OUT_MAX)

I calculated the inductor base on above condition.

Why in webench showing 12 uH? But I calculate using formula it coming 8.2 uH?

Additional question, If the load current is 0.5A, Should I use 2A rated current or 0.5A load current in formula to calculate?Should I use 2A rated current or 0.5A  load current in webench input?