Tool/software:
Hello,
I am testing the TPS2662 eFuse capabilities in order to replace it with a high side pMOS switch. My duty is to protect this high side switch from overcurrent condition (which is pretty impossible with a simple pMOS).
This is the circuit:
I don't use the UVLO and OVP capabilites so I disable them by default. I haven't placed a capacitor in dVdT as it may be left floating (I will cover it later).
With 12V in VIN it works pretty fine, I have monitored the nFLT signal with a oscilloscope but I don't have captures cause the IC is blown :(
But when I turn VIN higher (24V) the IC burns out. I suspect that this may be related to the soft start feature of the dVdT pin. The higher the voltage the higher the slew rate, so maybe with the default internal value the slew rate at 24V may damage the IC.
I haven't either placed capacitors in IN and OUT cause the circuit is just a prototype.
Can someone please tell me if I am right or the error may be other thing.
The exact PN of the IC is TPS26621 .
Best Regards,
Gorka.