I'm designing a high-power UCC2893-based supply with a CT for sensing current. In my system, the PWM IC isn't right next to the CT because of large components and the heatsink.
What parts should go near the CT and what parts should go near the IC? My current sense scheme looks like page 27 of the datasheet (http://www.ti.com/lit/ds/symlink/ucc2891.pdf), with the CT on the drain of the main FET. I'll use those ref des as an example. In a previous design using the same IC and CT, I placed R7 near the CT and everything else near the IC. I ran the traces from R7 as a diff pair to D1 and the plane of the IC. That worked OK, but waveform fidelity wasn't exemplary.
In my current design the CT is ~2" from the IC. Should I repeat the same component arrangement as above? Put everything except for R6 and C5 near the CT, with the RC filter near the IC?
Of course I looked at UCC2891EVM / HPA034. It doesn't exactly have this issue because the CT and IC are so close together there's just enough room for the parts.