Tool/software:
Guys
The typical circuit for synchronizing the UCC2818A-Q1 to an external clock is shown in figure 7 in the specification and is based on adding a pulse on the voltage on CT. The maximum value of the ramp peak voltage in the specification is 5,5V. To ensure synchronization the pulse has to be over 5,5V. The "Absolute Maximum Ratings" for the UCC2818A-Q1 does not include the maximum value of the voltage at CT. Is there any "Absolute Maximum Rating " given for the voltage at CT?
Regards
Kolbein