Other Parts Discussed in Thread: BQ25750, BQ25798
Tool/software:
I would like to use the USB-PD-CHG-EVM-01 in a test application for testing mobile charging bricks and other charging devices. I was wondering if the USB-PD-CHG-EVM-01 can be programmed to negotiate at a certain power level, such as 20 VDC @ 5 amps, etc., so that when it was connected to a device under test, it would discharge the device at that power level.
Also, I was wondering if there is an API that can be used to access the USB-PD-CHG-EVM-01 by a custom program so that I can automate the use of this device during a test.
Thanks in advance for all your help.
Regards,
Dayle Swensen