This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5880-Q1: Creepage disctance vs IEC 60664-1

Part Number: UCC5880-Q1

Tool/software:

Hi,

the external creepage distance of this device is 8mm. According to IEC 60664-1, 850V systems require 4.3mm.
Safe isolation (double base isolation) thus means 8.6mm distance, which is more than the datasheet states.

How does TI argument that this device can be used in 850V or even 1000V applications?

Best regards