Tool/software:
The starting current of the tps63060 is 2.4A, the input voltage is 6V, and the output is 5V. Is it normal?
The problem now is that the input power supply is an alkaline battery. When TPS63060 starts, the current is too large, which will pull down the voltage of the alkaline battery. Since the alkaline battery also supplies power to the MCU, the MCU will keep restarting after the voltage is pulled down, how to solve it?