Other Parts Discussed in Thread: BQ25180, BQ24133, BQ25185, TPS63020, TPS63060, TPS63070
Tool/software:
Hi,
I need help in selecting a lipo battery charger. I have micro hydro generator with the following specs.
-
DC5V Technical Parameters:
- Maximum Output Current: 100mA
- Max Output Voltage: 6V DC (with water flow at 10L/min)
- Standard Output Voltage: 5V DC (with water flow at 4L/min)
- Starting Output Voltage: 3V DC + 0.25V DC (at water flow of 3.5L/min)
-
Operating Conditions:
- Flow Range: 2 - 10 L/min (water pressure 0.05-0.2 MPa)
- Maximum Water Pressure: 1.2 MPa
- Temperature Range: 0 to 80 °C
- Ambient Temp Tolerance: Up to 100 °C (for 30 minutes)
- Storage Temp: -25 to 65 °C
I need a lipo charging IC that can charge 1Ah lipo battery. It would be great if it has regulated power output sharing feature as well.
The turbine will run through a water shower system so the power might not be consistent always.
I need very simple solution but not very complex. Power loss will be the key factor so minimal power loss.
Let me know if you have any other questions.
Thanks