Other Parts Discussed in Thread: LM5145
Tool/software:
Hello support team,
I am currently using the LM5145-Q1 to design a buck converter that generates 5V/12A from an input voltage range of 7V to 40V.
The enable pin of the LM5145-Q1 is connected to a resistor divider network powered by the same input voltage, through a p-channel MOSFET controlled by a signal from the MCU. This setup is designed to handle both the enabling and UVLO functionality simultaneously.
When the LM5145-Q1 is turned on, the buck converter operates as expected. However, when I disable the converter (by disconnecting the input voltage from the resistor network), the power supply turns off, but the output drops to approximately 1.2V to 1.3V. The 5V loads connected to the converter are off, but I am unsure why the power IC still generates this residual voltage after it has been disabled.
For ILIM sensing, I am using the Rdson of the low-side MOSFET. I came across a previous comment suggesting that the ILIM current source may pass through the output capacitors. Could this be the cause of the issue? If so, how can I resolve it?
This behavior has been observed consistently across all tested samples.
Despite this issue, the converter performs well in other aspects: the output is regulated under no-load, light-load, half-load, and full-load conditions. Additionally, startup, soft-start, step-load regulation, and line regulation are smooth, with no overheat problems, and the efficiency is satisfactory. The PCB layout is done on a single side with four layers, including two internal ground layers.
I would appreciate any guidance or suggestions you can provide.
Best regards,
Malek Hattab