Tool/software:
I have an application where i need to configure LDOREGOUT to 3.3V when fault in BQ76907 occurs and otherwise 0. this is to enable power for MCU. I know this is not possible as its an onetime programmable. Could you please see if any of the following ideas will work to acheive the same and if so how excatly can i implement-
1) can i switch modes(eg deepsleep to normal) based on fault occuring and will that read program again and set 3.3V. Will this work
2) can i use the programmable timer to work as per my requirement