Tool/software:
Hello Team,
My customer has below questions for LMQ66430-Q1. Could you please answer?
1. She is using LMQ66430-Q1 for application : Vin 12V, Vout 7.5V and Iout 0.6A.
Can she use external components in yellow from below table other then feedback capacitors? Please let me know if you have any concern.
2. LMQ66430-Q1 datasheet recommends X7R or higher grade MLCC for output capacitor.
She wants to use below capacitor part in her capacitor pool but it's X7S. Is it strict requirement? Or X7S can be acceptable?
CAP-C-C,22UF 25V K X7S 3225 -55TO+125 CL32Y226KAVVPNE / Samsung electrics
3. The minimum Input capacitor is 4.7uF as recommended in the typical component table.
She is using 2x 4.7uF capacitors on the input. Is it sufficient? Or, 2x10uF is more recommended as FIgure 8-1?
CAP-C-C,4.7UF 100 K X7R 3225 OPEN-MODE 12101C475K4Z2A / Kyocera
Thank you in advance.