Tool/software:
The controller is configured to accept input voltage between 9V and 20V. (ADC1 and 2 are configured for 9 and 20V)
When I connect 5V (from USBA) connector I see 5V on the PPHV, which I was not expecting when input voltage(5V) is below the lower limit voltage(9V).
So, there is no power negotiation and still 5V goes through VBUS to PPHV. Can you help to explain this situation?