Other Parts Discussed in Thread: TPS61500
Tool/software:
Does the LED Part Number LM3530 is only for White LED Applications? In the datasheet I can see the product description as White-LED Driver
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Napa,
It is ok to use this part if the specs can meet your need. I can help to check if you can send me your application conditions.
BR
Patrick
Hii Patrick Yao,
It's great to see you here!!
I'm Looking for a LED Driver with ALS for IR LED Applications. The LEDs will be turned OFF during morning & the LEDs will be turned ON during night.
Please find the Maximum rating of the LED that we are going to use
Forward Voltage: 2 V
Working current: 250 mA
Max pulse current: 1 A
Reverse Breakdown voltage: 5V
Power Dissipation: 500 mW
Operating Temperature: -30 to 85 degrees centigrade
Kindly help us in knowing the appropriate part number for the same.
Hi Napa,
So there will be only one IR LED? What is the input voltage range? Looks like you may need a buck LED driver.
BR
Patrick
Hii Patrick,
There will be around 10 IR LEDs connected in series.
Forward Voltage Range is 1.5 - 2 V
Thanks,
Karthik
Hi Karthik,
OK, so is the 250mA the real current your application will need? I need to know the maximum continuous current to choose the best solution.
BR
Patrick
Hi Karthik,
TPS61500 is also a good fit for this application. And for the Max pulse current 1A, do you have the data of what is this pulse width and period/frequency?
BR
Patrick
Hii Patrick,
At present I don't have the Pulse Width and Frequency details.
We are actually looking for IR LED Driver with ALS option. Is TPS61500 having ALS feature ?
Regards,
Karthik
Hii Patrick,
LM3530 has Max LED current of around 30 mA. But our LED has a Forward current of around 250 mA.
Hi Karthik,
Currently we don't have device with ALS and could also support 250mA LED current. Are you able to split the ALS function maybe to another IC?
BR
Patrick
Hi Karthik,
Our expert is currently out of office and will reply to you next Monday when back to office. Thanks for your understanding.
Best Regards,
Steven
Hi Napa,
If so, TPS61500 is able to be the LED driver for your configuration.
BR
Patrick
Hii Patrick,
Thanks for letting us know. Can you kindly suggest an ALS as well that works at input voltage of 5V? We want to use common voltage domain for both LED driver & ALS.
Hii Patrick,
We are in process of creating PCB footprint for this IC since we have a huge requirement. We are unable to get the required details regarding dimensions etc in order to create footprint. Can you kindly help us on this.
We want to get few samples from TI for this IC. But website is showing few errors even if we have entered all the details correctly. Kindly help us on these.