This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22997: Quick Output Discharge max. Current

Part Number: TPS22997


Tool/software:

Hello,

I have a question about the TPS22997. In the datasheet it says that the Quick Output Discharge (QOD) pin is typ. 50R to GND when the load switch is switched off. The 50R being realised as an internal FET.

How much current is the QOD pin / the internal FET able to handle? I cannot find a value in the datasheet. I am afraid that it could cause a problem to connect the QOD pin directly to my 5V output voltage when there is quite some capacitance on that voltage that would discharge through QOD potentially damaging the device due to over-current / -heat.

Thanks in advance.

Best regards, Jakob