Part Number: TPS65000-Q1
Other Parts Discussed in Thread: TPS65000
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65000-Q1
Other Parts Discussed in Thread: TPS65000
Tool/software:
Hi,
There should not be an interruption in the transition from PFM to PWM mode.
Please refer to the expected waveform in the datasheet:

This SW shutdown behavior may be indicative of another issue.
I believe I am in contact with an FAE looking this same issue - Jerry Hu? Can you confirm?
Best Regards,
Sarah
Hello,
Thank you for providing the images. It appears that there is a correlation between the mode switching and the voltage drop.
However, the mode switching itself should not cause this significant drop.
I would like to try to figure out why the device is switching, is there a change in load at this time?
What is the expected load current on this rail?
Best Regards,
Sarah
Hi,
Can you tell me more about the 60 mA load being connected to the 1.2V rail at this time?
Is it possible to try increasing the output capacitance at the 1.2 output rail to 22 uF to see if this helps with the drop?
From waveforms that Jerry Hu shared with me, it also appears there is a small drop in the VSYS and 2.8V output at this same time
and there was no/low input capacitance for VINLDO1 & VINLDO2.
Please add at least 2.2 uF to the input for best operation.
Best Regards,
Sarah