This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62873: Ramping up the output voltage doesn't follow the datasheet.

Part Number: TPS62873

Tool/software:

Hi team,

My customer has been evaluating start up voltage function based on the EVM(TPS62873EVM-144). My customer writes VSET[7:0](0.6V) and VRANGE[3:2](1.25mV steps) to TPS62873 via I2C interface after Input power supply of 3.3V gets stabled. And then TPS62873 is enabled.

Based on the datasheet, After EN is high, the output voltage first ramps up to the target voltage set by VSEL pin, and then new programmed value are set. In my understanding correct?

But actual evaluation on the customer's side, after EN is high the output voltage first ramps up to the target voltage set by VSEL pin. That's all. By making EN low and high again, the output voltage ramps down to new programmed value.

Could you please kindly let me know which one the correct operation is?

Best regards,

Shunsuke Yamamoto