Tool/software:
Hello,
My question is regarding the static sink current capability of the DESAT pin in the ISO5852S-EP part. The datasheet specifies that the Blanking-capacitor discharge current can range from 9mA (min) & 14mA (typ). Are these currents steady state ratings (continuous current) or dynamic, since it is specified as capacitor discharge current?
The background for my question is, we are seeing a continuous sink current of ~5.5mA into the DESAT pin (refer the below simulation image). This can be continuous when the gate driver is off & there is an internal MOSFET structure to sink the current in the DESAT pin. So we had a question about the reliability of the IC/pin. The 14mA spec given in datasheet is continuous or peak values?
In general when only DESAT capacitor discharges, it is a short spike in current.
Thanks.