Other Parts Discussed in Thread: TPS2640, TPS2660
Tool/software:
Hi team,
I want to use eFuse TPS259474LRPW in our application to monitor the voltage of a pure resistive load (~1.7 amps).
The response to fault is latch-off and I want to mainly use the eFuse to monitor the voltage input voltage and disable the load if the input voltage goes above 20V.
There are 2 possible conditions:
Input voltage is 17V = eFuse is on, load is powered.
Input voltage is 24V = eFuse detects overvoltage (>20V), latches-off, load is off.
The input voltage of 24 V can be sustained for long periods of time - (e.g. 30 days).
My question is around the recommended operating voltage (23 V), and the absolute maximum voltage (28V).
The 24 V of our application is within the absolute maximum, however it is above the 23V recommended.
I would like to understand why 23V is the recommended voltage and if the limitation of the part under this condition is applicable to my application:
- Is this 23V a number based on the maximum power dissipation under clamping mode/active current ? (this will not be the case for my application, then the 1V extra won't be a problem).
- Or is it a limitation of the breaking down voltage of internal circuitries and long-term reliability?
- Is it okay to have 24 V applied permanently with the overvoltage lockout protecting the load permanently?
Thank you.
Ede.