This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5141-Q1: LM5141-Q1

Part Number: LM5141-Q1

Tool/software:

HI,

We are using LM5141-Q1 in one of our projects and designed to generate 12V .When we turn on the board at start it generates 5V instead of 12V. But when ECU is restarted meaning hard reset is applied it generates 12V as expected.

Feedback resistor and Soft start Capacitor values are correct according to 12V design calculation and we are able to get 12V output once ECU is restarted but not during the first power on.

Design values used for 12V

Feedback resistor -100k , 11k

Softstart capacitor value_56nF

Can you please comment on this issue and suggest the solution how to rectify.