This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952EVM: BQ76952

Part Number: BQ76952EVM
Other Parts Discussed in Thread: BQSTUDIO,

Tool/software:

Hi, We are trying to use BQ7695204 IC in BQ76952EVM board so that the default communication can be SPI. But after changing the IC and jumpers for SPI communication, the EVM is not being detected in BQStudio tool. Also REG1 output is showing only 1.1V instead of 3.3V. Could you kindly suggest what could be wrong. REGIN is coming as 5.5V and REG18 is coming 1.8V.