Part Number: BQ79616-Q1
Other Parts Discussed in Thread: BQ79616, USB2ANY
Tool/software:
Dear TI support team,
I am involved in the hardware development of our battery management system using the BQ79616 and BQ79600 with a STM32 for our Formula Student vehicle.
We have recently received our custom developed boards and have problems connecting using the provided BQ auto EVAL software in testing. We are trying to wake the device using UART, we are able to send the wake ping on RX pin of the device however see no response on the TX pin. The LDOIN supply is 4.6V but both DVDD and AVDD both measure 0V.
Our concerns is the device is latched in a shutdown mode and we have two possible theories. Firstly being a communication fault when communicating using the USB2ANY through the wake procedure. We have added relevant 1k termination resistors across all unused COMM channels during the single board testing, but the issue persists. The second potential reason we believe the device isn't working because of it being in a permanent thermal shutdown state due to hand soldering at 350 degrees, however our interpretation is that thermal shutdown can only be triggered once the device is powered.
Your feedback would be highly valuable.
Thank you.