Other Parts Discussed in Thread: LM74930, , LM74502H
Tool/software:
Hello,
I have some questions on the LM74930.
It is not clearly in datasheet how to handle the OVCLAMP Signal.
Can you check, if my understanding is OK?
- OVCLAMP pulled to GND (OV connected to Input) => no overvoltage clamping => output switches off during overvoltage
- OVCLAMP connected to OV pin => in this case the output voltage is limited at overvoltage => OV voltage divider must be connected to output
- OVCLAMP connected to OV pin and voltage divider connected to input => output switches off during overvoltage (makes no sense due to clamp-function)
In the calculation sheet a "Required Maximum allowed Inrush Current" should be specified.
Our application has a resistive load current of up to 35A. Is this (or a value above) also the Inrush current for the calculation?
The Turn-on Gate currents are very low (55µA). I'm not sure, if this leads to a problem due to slowly switching MOSFETs.
The calculation don't checks the Gate charge of the MOSFETs.
We also want to use the Chip with a slow PWM application (about 1Hz or up to 10Hz).
Would this be possible via the Enable pin?
Can Simulation be done with the TI PSPICE simulator? Actually I'm not able to download the SW.
Best regards
Harald