This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: Varying the output from 13V/3.5A to 30V/11A

Part Number: LM5145
Other Parts Discussed in Thread: DAC63204

Tool/software:

Hello! 

I need a circuit that can vary the power delivered to a resistive load. The input is a consistent 48V, and the output needs to vary based on the desired current. I'm hoping that I can achieve this with the LM5145 and a DAC63204 injecting voltage into the FB network.

I  used WEBENCH to design a circuit for the top end, and it provided this:

WEBENCH (ID = A78FCE84726613A0)

I simulated a similar (higher top end) circuit in TINA with a voltage controlled feedback resistor, and it looks stable:

Is this feasible?  Am I heading down the right path here?  Any insight would be extremely appreciated, buck converter stability isn't in my wheelhouse.  

Thank you,

Jamie