The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS715: TPS715 OCP function

Part Number: TPS715

Tool/software:

Hi Team,

I am wondering if TPS715 OCP condition is for below ICL specs or another spec? Since TPS715 is a 50mA LDO and I am not sure the OCP can up to 90mA. Thanks.

BR.

Frank

  • Hi Frank,

    The ICL specs are accurate as indicated in the datasheet. 50 mA LDO means that it will perform as per the specs advertised in the datasheet for up to 50 MA of load current. This is the recommended max load current. Beyond this, TI cannot guarantee an adherence to the specs in the datasheet. The current limit kicks in as a brickwall and the value of I_CL is shown in the EC table.

    Regards

    Ishaan