Part Number: TPS54202
Tool/software:
The customer feedback that there is output voltage overshoot. Could you help to analysis it?
Yellow: Output voltage
Green: EN
Blue: Input voltage



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fabio
Can you please add SW waveform in the page and see is the switching stable during the start up ? And the soft start time should be 5ms.
Can you please also share the layout image?
Thanks and best regards.
The layout is as below

Hi fabio
Comments on the layout:
The feedback resistors(R403,R404) should be placed close FB pin, R404 should be placed close to FB pin and GND pin.
The Cin (C404) should be placed close to Vin and GND pins.
Thanks and best regards.
The green is the SW.
The yellow is the output voltage.
Why there is overshoot?

Hi Fabio
Seem from below image: EN seems is not the voltage divider from Vin, is it connected to other circuits?

The EN pin is connected to Vin.

Hi Fabio
EN is connected to Vin through a resistor divider seen from the schematic, but in the waveform, the EN slew rate changes t=t1, can customer check what happens after t1?

Thanks and best regards.