Tool/software:
Dear team,
Please help us to understand CS function of BQ79656.
Q1: Would I know the full scale range of CS delta-sigma ADC? Page#9 8.3 mentions it is VCS_RANGE = +/-100mV, but 9.3.2.4 mentions it is +/-125mV.
Q2: About 9.3.2.4, it mentions as shown below screen shot. Does it mean CURRENT_HI/MID/LOW will be below table? And How will it be when it is lower than -125mV (-100mV.)
< -125mV : -125mV (=0x000000) or -75mV
-125mV ~ -100mV: -125mV ~ -100mV
-100mV ~ +100mV: -100mV ~ +100mV (high accuracy)
+100mV ~+125mV: +100mV ~+125mV:
> + 125mV:75mV
Q3: Related to Q1, can BQ79656-Q1 measure current with CS ADC in accuracy within the range of +/-100mV, and relatively lower in -125mV to -100mV and 100mV to 125mV?
Q4: What is the 0x0000 of MAIN_CURRENT_HI/LO? Its LSB is 30.52uV but not sure its absolute value.
Q5: Same for CS ADC and CURRENT_HI/MID/LOW, its 0x000000 would be -125mV? which means 0x000fff is 0V?
Best regards,
Yuto