Other Parts Discussed in Thread: AMC1400,
Tool/software:
Hey team!
I recently got a client request for a system that needs a wide input AC voltage (220VACrms to 490ACVrms) for a 7kW setup. I’m using the UCC28070 device and following the guidance from the SLUA479 App note to make sure the power output is on point.
I’ve been digging around in the TI community and came across some interesting tips:
It looks like +5-10V mentioned that the output voltage levels need to be higher than the input peak voltage, which in my case is around 700Vdc. To reach that, I’ll need to play around with the sensing pins.
Right now, I’m using the SLUC114 - UCC28070 Excel App design tool. Is this spreadsheet reliable for the voltage range I’m working with? Can I trust the values it’s giving me for the sensing components?
I also calculated the current sense transformer, and it’s showing a turn ratio of about Ns/Np ~ 665. Would it be possible to use an isolated amplifier instead, say like AMC1400?
Is there anything else I should double-check while I'm at it?
Thanks for your support!